Deutschland  |  0800-8266342 Gebührenfrei

Troubleshooting Thermocouple Input Devices

Testing a thermocouple input measuring device is as simple as connecting a short across the input terminals. This applies to ALL thermocouple measuring devices, such as plug-in cards, dataloggers, panel meters, hand held meters, temperature controllers and recorders.

There are many factors that can give a thermocouple measuring device an erroneous reading, such as noise, ground loops and broken thermocouples. When encountering trouble measuring thermocouples, the first test should be the SHORT test, since it literally takes minutes and usually answers many questions.

For example, if a thermocouple is connected to a plug-in card (designed for thermocouple inputs), and erratic readings are noticed, it may be the result of a ground loop or noise induced on the thermocouple wires. It may also be a faulty plug-in card. At this point, there is a lot of uncertainty. Simply remove the thermocouple and connect a piece of copper wire across the input in its place (also, connect another piece of wire from the (-) to LL Gnd. If you have more than one thermocouple connected, remove ALL of the thermocouples and short all the active inputs. They should all read room temperature, and should be fairly stable. If the readings are stable and read ambient temperature when shorted, then we know that it is not the card, nor the PC, nor the software, but may be in the wiring or even a broken thermocouple. This will not solve all of your problem, however it is a simple first step that will help to narrow down the possibilities. If, on the other hand, the readings are still erratic, then it may be the board and it may need to be returned for repair. It would be a good idea to try another PC to eliminate the possibility of a bad PC slot or power supply, etc. Also, if a custom program is being used, it would be a good idea to test the board with factory supplied software.

If it is determined that the board works fine with a short, then the thermocouple wiring must be checked. Re-connect the thermocouple, and try moving the wiring around a bit. It is better to go a longer distance and work AROUND a noisy piece of equipment, such as a motor or compressor than to go directly over this equipment. Sometimes, it is necessary to use SHIELDED thermocouple wire, where the shield is connected to a suitable ground on ONE END ONLY.

Sometimes, it is necessary to completely electrically isolate the thermocouple from what you are measuring. If you are inserting a probe into a machine, there may be voltages present which can cause current to flow into the thermocouple right through its steel sheath, causing erratic readings. The solution is to use UNGROUNDED thermocouples, where the sensor does not touch the sheath, therefore isolating it. This may reduce response time a bit, but will stop any ground loops. If connecting a bare wire to a metal surface, a neat trick would be to use an non-conductive paint and cover the thermocouple tip, making sure the paint can handle your temperature range. Or, put a small piece of tape on the surface, or use OMEGABOND epoxy to isolate the wires. In extreme cases, or areas where tape or paint cannot be used, signal conditioners can be used to isolate a thermocouple up to thousands of volts. This is the most expensive method (average of USD$200 per channel) however, is the most fool proof, providing electrical isolation, noise filtering and signal amplification as well as safety. Since the signal is amplified to a higher voltage, or even 4-20ma, a less expensive card may be used instead of a thermocouple measuring card.




MMV | 6 |